FAQ Pencarian
Can I have two HMI's share variable data without a PLC in EcoStruxure Operator Terminal Expert?
Issue:
Can I have two HMI's share variable data without a PLC in EcoStruxure Operator Terminal Expert?
Product Line:
EcoStruxure Operator Terminal Expert. HMIST6, HMISTO7, HMISTM
Resolution:
As of EOTE 3.1 HF1, it is not a possible to configure with EOTE. It is only possible to have one HMI per project, and no associations between Targets.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Produk:
Jelajahi lebih lanjut
Produk: