The datasheets are good :
- AC13 P300 for the ZBE501 : 1,1A under 120V and 0,55V under 240V
- AC13 Q600 for the ZBE101 : 0,55A under 120V and 0,27V under 240V
The ZBE501 is done for higher current.
Diterbitkan untuk:Schneider Electric Indonesia


{}
The datasheets are good :
The ZBE501 is done for higher current.