{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you tell me the differences between the PM700 Power Meter range ?

Article available in these languages: French, Dutch

The PM 700, PM700P, PM710 & PM750 all provide the following readings

  • Voltage of each phase, current in each phase
  • Real, active, apparent power per phase
  • Frequency, Power Factor
  • Active, apparent, relative energy (kWh, kVaR, kVArh)
  • Current demand, power demand
  • min /max of instantaneous readings
  • Voltage THD (Total harmonic Distortion)
  • Current THD(total Harmonic Distortion)


The PM700 is a 3 phase multi function meter with no RS485 Modbus communication and no pulsed outputs
The PM700P is a 3 phase multi function meter and has pulsed outputs but no RS485 Modbus communication
The PM710 is a 3 phase multi function meter  and has  RS485 Modbus communication and no pulsed outputs
The PM750 is a 3 phase multi function meter and has pulsed outputs and RS485 Modbus communication

Please note the PM700 range is now obsolete, for information on replacement please see FAQ FA264122

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top