{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why I cannot communicate with a Power Meter (PM5100, PM5110, PM5111, PM5300, PM5330) from a remote personal computer?

There are several common causes and solutions:

1. Possible Cause

The Power Meter address is incorrect

Possible Solution
Check that the Power Meter is correctly addressed, each meter on the same bus should have a unique address.

2. Possible Cause
Power Meter baud rate is incorrect

Possible Solution
Verify that the baud rate of the power meter matches the baud rate of all other devices on its communication link.

3. Possible Cause
The parity is incorrect

Possible Solution
Check the parity on all the meters are the same on the communication link.

Note: This is not an extensive list, for example; it is always good to check if the physical cable and connections are healthy.
Another approach is to check another meter, and complete exclusive tests to identify the fault

Schneider Electric Ireland

Attachment(s)

PM5000 series meter instructions.pdfPM5000 series meter instructions.pdf [2.98 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: