{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the default IP address of the TSXETZ Ethernet gateways?
The default Ethernet interface IP address for the TSX ETZ module is derived from it’s MAC address which is printed on the ETZ module:

085.016 is common to 'all' ETZ modules.


085.016.xxx.yyy where xxx and yyy are the last two numbers of the MAC address.


Example

The module’s MAC address is (in hexadecimal): 00 80 F4 01 12 20
In this case the default IP address is (in decimal): 085.016.018.32
Note:
This platform is discontinued. Please get access to our digital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform.

Schneider Electric Ireland