How can we help you today?
What is the maximum earth loop Impedance Zs value for the circuit breakers used in the Powerpact 4 panel board?
The maximum earth loop Impedance figures can be found on the attached pdf files.

16A to 250A
The standard MCCB's used for ratings of 16A to 250A with part numbers beginning with "MGP..." are identical to the NSX with thermal magnetic trip units.


400A & 630A
The standard MCCB's used for ratings of 400A & 630A with part numbers beginning with "MGP..." are identical to the NSX with Micrologic 2.3 trip units.

Schneider Electric Ireland

Attachment(s)
Zs Values Compact NSX With TMD Trip.pdf [53.23 KB]
Zs Values Compact NSX With Micrologic 2.2.pdf [505.86 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.