{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the differences within the TSXETG3000 Ethernet Gateways product range?

These products are free standing modules that can be implemented into an Ethernet Network. All of these modules require configuration with Web Designer software supplied with module. The units are classed as Factory CAST HMI products as they can have custom web pages added, . Custom web pages can be created using Microsoft Front page. The TSXETG3000 range of gateway are all Class D20 embedded web server. Factorycast HMI adds services such as E-mail,

They included a gateway to enable you to connect onto either a Unitelway bus, or Modbus bus depending upon the hardware you use :-

TSXETG3000 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality, configured with Web Designer s/w supplied with module

TSXETG3010 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality + PSTN Modem and embedded I/O board

TSXETG3021 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality+ GSM Modem 900 / 1800MHz (UK and European Market) and embedded I/O board

TSXETG3022 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality + GSM Modem 850 / 1900MHz (US and Canada and South American Market) and embedded I/O board.

For further details see summary of functions document attached.
Note:ued. Please get access to our From the catldigital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform.

Schneider Electric Ireland

Attachment(s)

TSXETG3000 Factorycast Gateway summary of functions.pdfTSXETG3000 Factorycast Gateway summary of functions.pdf [30.3 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: