{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the percentage impedance guarantees of the Distribution Transformers?

The Fast Trans range of transformers, which are liquid filled free breathing distribution transformers, covers following kVA ratings and the percentage impedance guarantees for each rating as detailed below :-

315kVA           Percentage impedance guarantee = 4.75% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
500kVA           Percentage impedance guarantee = 4.75% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
800kVA           Percentage impedance guarantee = 4.75% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
1000kVA         Percentage impedance guarantee = 4.75% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
1250kVA         Percentage impedance guarantee = 5.0% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
1500kVA         Percentage impedance guarantee = 5.5% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
1600kVA         Percentage impedance guarantee = 5.5% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%
2000kVA         Percentage impedance guarantee = 6.0% at a Reference Temperature of 75ºC, subject to IEC 60076 Tolerances of ±10%

Schneider Electric Ireland

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: