Search FAQs
Can I use hit and run on ADVC recloser control cubicle?
Operators can now introduce a time delay between pressing either the Trip or Close buttons and the Recloser or Load Break Switch actual operation of.
This feature can be useful within substations for operators who are required not to be in the vicinity of a device when it operates. This feature must firstly be enabled via WSOS whereby it becomes an option for the local operator.
This feature can be useful within substations for operators who are required not to be in the vicinity of a device when it operates. This feature must firstly be enabled via WSOS whereby it becomes an option for the local operator.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: