{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the differences between T200I and T200E?

Functionally there are no differences between the two RTU's.

The key differences are: -

  • IP rating of T200I is IP41
  • IP rating of T200E is IP54
  • T200I is limited to controlling 4 functions
  • T200E can control up to 16 functions
  • T200I has Harting type connectors underneath the cubicle for the switchgear umbilical's
  • T200E has special sockets inside the cubicle on the interface card


For more information on T200I and T200E click here

Schneider Electric Ireland