Search FAQs
Can I use other manufacturers PTC probes with the LT3S*?
The PTC thermistor probes used with the LT3S are manufactured according to the following standard ( see catalogue )
- Label mark A conforming to IEC 60034-11
- It is possible to use any probe which conform to this standard.
- It is possible to use our probes on any product which are manufactured according to this standard .
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: