{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the definition of an auto-transformer?

An auto transformer is a transformer in which at least two windings have a common part.
In an auto transformer, one single winding is used as primary winding as well as secondary winding.
Alternatively in two windings transformer two different windings are used for primary and secondary purpose.

Schneider Electric Ireland

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: