{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the definition of no-load current of a transformer?

The RMS value of the current flowing through a line terminal of a winding when rated voltage (tapping voltage) is applied at rated frequency, meantime the other winding or windings being open circuited.
NOTE 1. For a three-phase transformer, the value is the arithmetic mean of the values of current in the three phases.
NOTE 2. The no-load current of a winding is often expressed as a percentage of the rated current of that winding.
For a multi-winding transformer this percentage is referred to the winding with the highest rated power.

Schneider Electric Ireland

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: