{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find information covering the LE1GB, LE2GB or LE3GB enclosed DOL, reversing and star delta starters?
NOTE: The mentioned ranges are now obsolete, this information is kept for legacy purposes only.

The LE1GB, LE2GB or LE3GB enclosed DOL, reversing and star delta starters are only marketed in the UK, for this reason the information on our website is limited.

This range of enclosed starters are IP65, have a robust metal base and a polycarbonate cover.
Versions are available with or without a disconnect switch.

Attached to this FAQ you can find a catalogue extract and the instructions sheet  for the range (see bottom of page).

Important notes:

These starters are supplied without thermal overload relays fitted.
Separate overloads should be selected as follows based on the motor full load current (FLC) or in the case of the star delta starters the FLC x 0.58.

Starters LE*GBK use LR2K* thermal overload relays, starters LE*GBT use LRD* thermal overload relays as detailed below;

Overloads for LE1GB



Schneider Electric Ireland

Attachment(s)
LE1GB LE2GB LE3GB.pdf [138.31 KB]
Instructions.pdf [132.87 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.