{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do I interpret the instruction sheet for Osiconcept (Multi-mode) Photoelectric detectors?

The instructions are designed to be, as far as possible, language independent so are primarily graphical rather than descriptive. As a reminder to an individual who is already familiar with the product this works well, but it can prove difficult for a user to understand if it is their first experience of the system.

Attached to this FAQ is a set of text instructions which on their own should be sufficient to explain the required processes, but are particularly useful when used alongside the graphical instructions supplied with the unit which are also attached.

Schneider Electric Ireland

Attachment(s)

XUB XUM XUK XUX Data Sheet bbv13273.pdfXUB XUM XUK XUX Data Sheet bbv13273.pdf [1.14 MB]
Setting Up Osiconcept.pdfSetting Up Osiconcept.pdf [24.23 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: