{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where can I find product substitution (cross reference) information to help with converting old part numbers to new equivalents?

Article available in these languages: Czech, Slovakian

On the Schneider-Electric UK web site there is a product substitution tool to help with converting old part numbers to new equivalents.
The first step should be to use this tool to check if the old part is listed as a high percentage of the old parts have been included.

Important notes concerning product substitutions;
  • The tool will suggest the nearest equivalent from the current range of products.
  • The substitution product may not have all the functionality of the original so do check the suggested replacement meets the requirements of the application.
  • When using equivalents it is often necessary to substitute more than one part, e.g. replacement of both bodies and heads in the case of manual control devices and in the case of contactors with overloads.
  • Equivalent products will often be of different dimensions with connection terminals in different locations, as a result modifications to the installation may be required to accomodate the replacement product.
To locate the tool use the following link;

https://www.se.com/uk/en/product-substitution/

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.