{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the programming cables required to connect to a Twido controller?

To communicate over USB to a Twido PLC, use a USB to RS485 converter ref TSXCUSB485 and cable ref TSXCRJMD25.
Note:
The Twido range is discontinued and the possible replacement is the Modicon M221. The software to program this new controller is the EcoStruxure Machine Expert Basic also free.
The software can automatically be migrated to this new platform but check with our support center your architecture to validate the migration.
You can also use our product substitution tool to help you select the replacement for the twido:  https://www.se.com/ww/en/product-substitution/

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: