Search FAQs
What replaced XPSAS? What are the differences between XPSAS and the new XPSAF?
NOTE that XPSAF has now been replaced by XPSUAF. Please see attached document for further information.
XPS-AS Replaced by XPS-AF
XPS-AS Replaced by XPS-AF
XPSAS (old model) XPSAF (new model)
- XPS-AF has one extra N/O safety output
- XPS-AF is 22.5 mm width
- XPS-AS has larger range of voltage selection
- XPS-AS can be used for Type III A two-hand control monitoring
- XPS-AF has choice between 2 models with or without removable plug terminals (P)
- Schematic ComparisonsMonitoring of E-stop with 2N/C contacts
Monitoring of E-stop with 1N/C contact
Monitoring of E-stops with 2N/C contacts in series
Monitoring of a movable guard associated with 2 limit switches with 1 contact each
Cross Reference Table
NOTE: Data sheets about new safety relays XPSAF are available on the web site to download, use the search engine (top right corner)
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Range:
Explore more
Range: