Search FAQs
Will GV2, GV3 and GV7 get de-rated with altitude? How will the de-rating work?
For GV2, GV3 and GV7:
Yes, for altitudes higher than 2000m, see below the de-rating on this table:
For GV4, GV5 and GV6:
Yes, for altitudes higher than 2000m, see below the de-rating on this table:
Yes, for altitudes higher than 2000m, see below the de-rating on this table:
Altitude | Ue | Ie |
≤ 2000m | 1 (no de-rating) | 1 (no de-rating) |
2500 m | 0,9 | 0,92 |
3000 m | 0,8 | 0,90 |
3500 m | 0,7 | 0,88 |
4000 m | 0,6 | 0,86 |
For GV4, GV5 and GV6:
Yes, for altitudes higher than 2000m, see below the de-rating on this table:
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: