{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What Schneider Electric Drive has replaced the Telemecanique Altivar ATV28?

There have been several revisions of drives since the ATV28 was made obsolete. Therefore, it is best to consider the requirements afresh.

The current range that may be acceptable as the evolution to the ATV28 drive would be the ATV320 range, however if the old drive used was a single phase input to three phase output the ATV12 drive may be a suitable replacement if no braking resister required on the application.

Either download the catalogue for the ATV320 or ATV12 range to find a suitable drive or contact Schneider Electric and we will assist you in selection
If you need support in selection it would be useful to have the following information available:

  • Motor kW or HP rating?
  • Motor Voltage?
  • Motor Current?
  • Application (eg Machine, Pump, Fan etc)?
  • Load type or Torque Requirements (Variable or Constant)?
  • Input voltage and number of Phases?

This is not an exhaustive list, but will assist in directing to a suitable replacement or new drive.

The drive that replaced the ATV28 range was the ATV31 range ,which was then replaced by the ATV312 range, this in turn has now been replaced by the ATV320 as the evolution path.

Schneider Electric Ireland

Explore more
Range:
Altivar 312Altivar 12Altivar Machine ATV320Altivar 32
Explore more
Range:
Altivar 312Altivar 12Altivar Machine ATV320Altivar 32
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.