What size padlock can i use on the NSX MCCB lock off device 29370?
The NSX MCCB lock off 29370 padlocking system will accept up to three padlocks with shackle diameters ranging from 5 to 8 mm. Compatible with the NSX, MGP CDXAE, CNXAE CHXAE range of MCCB's.
Released for:Schneider Electric Ireland
Explore more
Range:
ComPact NSX
Compact NG160
ComPact NSXm
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.