{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Types of control for a KNX lighting system
(Legacy product)
The interior and exterior lighting of a building can be switched or dimmed individually, in groups or from an unlimited number of locations. The operation is carried out manually via KNX push buttons, remote control via radio as well as automatically dependent on time, brightness and movement via automatic detection of people in the vicinity.

Schneider Electric Ireland