{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Which Quadbreak cable box do I require?

The following chart provides the product code of the recommended cable box for each rating of Quadbreak fuse switch disconnector

63ASQBX100
100A
160ASQBX160
200ASQBX250
250A
315ASQBX500
400A
500A
630ASQBX630
800A

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: