{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum split configuration on the new 16 way flexible split load Easy9 Consumer unit EZ9FS16CU ?

The maximum split configuration on the 16 way flexible split load Easy9 consumer unit has a Max of 4 unprotected, Max of 9 on RCD 1 and a Max of 9 on RCD 2. The values given highlight maximum ALLOWABLE ways only, the installer will only be able to achieve up to 16 outgoing ways with this product.

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: