Search FAQs
How is level detection of a liquid in a transparent bottle achieved using capacitive proximity detectors?
Capacitive proximity sensors utilise a non-contact capacitive coupling principle to detect any object irrespective of material or conductivity, for example metals, minerals, wood, plastic, glass, cardboard, fluids etc.
Liquid level detection in a transparent bottle is therefore possible using two capacitive sensors arranged as shown;
![Capacitive sensors Capacitive sensors](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H0000088Z7lQAE&oid=00DA0000000abSm)
Sensitivity adjustment of the sensor is performed using a small screwdriver as shown;
![LED placement LED placement](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H0000088ZAPQA2&oid=00DA0000000abSm)
Schneider Electric capacitive proximity sensors (XT1 type) are available in 12mm through to 32mm diameter sizes with nominal sensing distances of 2mm through to 15mm respectively.
Liquid level detection in a transparent bottle is therefore possible using two capacitive sensors arranged as shown;
Sensitivity adjustment of the sensor is performed using a small screwdriver as shown;
Schneider Electric capacitive proximity sensors (XT1 type) are available in 12mm through to 32mm diameter sizes with nominal sensing distances of 2mm through to 15mm respectively.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: