{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the possible causes of the SCF fault of a variable speed drive from the Altivar range?

An SCF fault is generated by the drive if a motor short-circuit fault (to ground or phase-to-phase) occurs. Because of the nature and the destructive effects of this fault, this information is treated as a priority and is handled locally by the power bridge of the drive, which immediately disables activation of its IGBT power components.

This fault cannot be configured or reset; it can only be stored for indication purposes.

Diagnostics
The fault normally occurs in the motor or cables and can usually be found using a 1000V insulation tester. .
To do this, first remove the supply from the drive and allow time for the voltage to decay, then remove the motor cables from the drive and check them with the Insulation tester. To earth this should be infinity.   The Phase to Phase value depends on the motor but the readings but it should be the same for all windings.

To carry out the phase to phase test you need disconnect the motor cables from the drive output, and drop the motor links out in the motor connection box for the star or delta connections to isolate the windings from each other, you can leave the motor cable connected and test with the insulation tester between the phases down the motor cable and motor as one test or disconnect the motor cable from the motor and test the motor and cable individually, as we need to confirm if there is anything tracking down between the cores of the cable or the motor windings from phase to phase.
On very rare occasions it could be a drive problem, to check this turn off the OPF and with the motor cables disconnected from the drive run the drive if you get the SCF fault appear it is a drive problem and you should contact Schneider Electric Technical support

On the larger drives the ATV61 , ATV71 , ATV600 and 900 series, you can test the IBGT module by following the instruction in the programming manual, which can be down loaded from our web site

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: