{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What cable do I need to connect a Zelio Logic smart relay (SR2/SR3) to PC?

The Zelio Logic range of smart, programmable relays have a special communication port which enables them to be programmed and set up using a PC.

The communication ports on a PC are usually USB or 9-way SUBD. Schneider sells cables that are able to adapt to both these types of port.

For the SR2 or SR3 relays:
  • SR2USB01: Connecting cable with USB type PC connector, length: 3 m
  • SR2CBL01: Connecting cable with 9-way SUB-D type PC connector, length: 3 m
An SR2CBL06 cable can be used to adapt the USB port of the SR2USB01 cable to the 9-way SUB-D port of the PC port and vice versa.

For the old SR1 range:
  • SR1CBL01: Connecting cable with 9-way SUB-D type PC connector, length 1.80 m.
    • Note that this component is obsolete - this is for information purposes only
Please note - The connecting cables are specific to a range, thus the PC - Zelio Logic connecting cables used for the SR2 or SR3 is incompatible with the SR1 range.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: