{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I connect a potentiometer on the RE7TM, TP, MA, RA, RM, PP, PM,ML or MY time delay relays?

Please note that this range is no longer available - this FAQ is for reference only. For the same functions the suggestion would be to use a Zelio Logic or similar controller.

When using RE7 TM, TP, MA, RA, RM, PP, PM,ML or MY relays with time delay adjustment potentiometers, the potentiometers must be connected in the following way:

  • The opposite ends of the potentiometer should be connected to Z1 and Z2
  • Wire the potentiometer wiper to Z2

The specification of potentiometers to be used for RE7 relays is as follows:
47K Ohm, Linear, 0.2W or greater. 
Wiring Diagram

Schneider Electric Ireland

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.