{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Degree of Protection (IP) of the protection enclosure for a TRIHAL transformer?

For indoors, the standard protection enclosure of the TRIHAL transformer is IP 31.
Non-standard and indoors - IP 23 enclosure for a polluted environment can be installed.
For outdoors and customised transformers - IP 35 minimum protection enclosure can be ordered.

Schneider Electric Ireland