{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the definition of the dials/ selector switches of the Micrologic and STR electronic control units.
Standard IEC 60947-2 defines the names of the selector switches.
The meanings of the screen-printed items on the selector switches of the trip units are:
Ir: adjustment of the long time (or thermal) setting.
This is a multiplication coefficient of the rating of the device. Role: protection against overloads.

tr: long time delay in seconds, enabling in particular the starting current of a motor to be tolerated.
Isd: short time ("magnetic" or "Im").
This is a multiplier of the Ir setting, often 1.5 to 10 times the Ir current. Role: protection against short circuits.

tsd: short time delay, enabling in particular the discrimination (time) to be increased with downstream feeders and the magnetization peaks of a transformer or a motor to be tolerated.
It is recommended that the I²t selector switch is set to the ON position.

Ii: instantaneous current. Role: protecting the installation against strong short circuits (dead short circuits) by instantaneous tripping and self-protection of the circuit breaker.
The li setting must be higher than the Isd setting.

Ig: Ground fault protection. Role: for monitoring the earth fault current circulating in the PE conductor in TNS systems.

tg: Ground fault protection time delay.

I delta n: adjustment of the sensitivity of the earth leakage protection (Micrologic 7.0 or Vigi module)

delta t: earth leakage protection delay.

Schneider Electric Ireland

What is the definition of the dials/ selector switches of the Micrologic and STR electronic control units.
Standard IEC 60947-2 defines the names of the selector switches.
 
The meanings of the screen-printed items on the selector switches of the trip units are:
 
Ir:  adjustment of the long time (or thermal) setting.
This is a multiplication coefficient of the rating of the device. Role: protection against overloads.

tr:  long time delay in seconds, enabling in particular the starting current of a motor to be tolerated.
 
Isd:  short time ("magnetic" or "Im").
This is a multiplier of the Ir setting, often 1.5 to 10 times the Ir current. Role: protection against short circuits.

tsd:  short time delay, enabling in particular the discrimination (time) to be increased with downstream feeders and the magnetization peaks of a transformer or a motor to be tolerated.
It is recommended that the I²t selector switch is set to the ON position.

Ii:  instantaneous current. Role: protecting the installation against strong short circuits (dead short circuits) by instantaneous tripping and self-protection of the circuit breaker.
The li setting must be higher than the Isd setting.

Ig:  Ground fault protection. Role: for monitoring the earth fault current circulating in the PE conductor in TNS systems.

tg:  Ground fault protection time delay. 

I delta n:  adjustment of the sensitivity of the earth leakage protection (Micrologic 7.0 or Vigi module)

delta t:  earth leakage protection delay.

Schneider Electric Ireland

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top