{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do Schneider Electric sell adapters to enable 22mm diameter pushbuttons and signaling devices to fit in to a 30mm diameter hole?

Schneider Electric has 2 adapters (reducer) available that can provide a solution to the requirement for mounting a 22mm pushbutton or other control and signaling device in to a 30mm cut out (hole in control panel / station). We also offer a flush range within our 22mm range, which requires 30mm mounting holes.

  • ZB4BZ012
  • ZB4BZ021/22 (Flush-mount)
  • XB4 / XB5 Flush range (30mm mounting as standard)

ZB4BZ012

This adapter enables any standard 22mm device from our XB4/XB5 catalogues such as the 'Harmony' ZB4BA3 + contact body sub assembly, to be mounted in a 30mm cut out.

ZB4BZ012


Flush mount: ZB4BZ021 for pushbuttons and pilot lights / ZB4BZ022 for selector switches and illuminated pushbuttons

This adapter enables a standard 22mm pushbutton such as the 'Harmony' ZB4BA3 + contact body sub assembly to be mounted flush with bezel in a 30mm cut out.
ZB4BZ021/022


Flush range XB4/XB5

We now offer a flush range within both our XB4 Metal and XB5 Plastic ranges, which require 30mm diameter mounting holes as standard (without the use of mounting kits).
Please see our catalogue for details on this range: Control and signalling units Harmony XB4 Metal or Harmony XB5 Plastic

You can find our digital catalogues here: digicat.se.com

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: