{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many ASi slaves are managed by the TWDNOI10M3 ASi master module?
The TWDNOI10M3 module is an AS-Interface master modulefor Twido PLC or Modicon M238 (TM238LFDC24DT•• or TM238LDD24D T or TM238LFAC24DR•• or TM238LD A24DR)

The TWDNOI10M3 module can managed 31 standard address slaves or 62 extended address slaves. Regarding the cycle time 5 ms for 31 standard or extended address slaves or10 ms for 62 extended address slaves.

Attached in this FAQ we can find the Hardware Guide.

Note: The Twido range is discontinued and the possible replacement is the Modicon M221. The software to program this new controller is the EcoStruxure Machine Expert Basic also free. The software can automatically be migrated to this new platform but check with our support center your architecture to validate the migration. You can also use our product substitution tool to help you select the replacement for the Twido: https://www.se.com/ww/en/product-substitution/

Note 2: The ASi is not supported in the M221 range. You should probably check a new architecture with the BMXEIA0100 if you still want to use ASi

Schneider Electric Ireland

Attachment(s)
Modicon TWDNOI10M3_EIO0000000608.03.pdf [549.34 KB]