Search FAQs
Which product replaces the XCKJ59 safety interlock switches?
Please note - As of 01/09/23 the Telemecanique Sensors range is no longer part of Schneider Electric. This FAQ is now for reference only. For further information and contact details for Telemecanique Sensors, visit their website. They are now an independent company.
The nearest direct replacements for XCKJ59xx safety switches with interlocking and electromagnetic locking are the XCSLxx range.
XCKJ59xx was available in many variations of solenoid connector and actuator orientation as well as coil voltages and cable gland threads. Not all these combinations are available in XCSLxx switches, but there is usually one close enough for most applications.
There is also a much more up to date range of metal or plastic safety switches with solenoid locking/unlocking, the XCSExx and XCSTExx ranges. However, whilst these perform a similar function the physical design is quite different and may require modification of the machine/mountings to replace XCKJ59xx. Please see the attached document for details.
The nearest direct replacements for XCKJ59xx safety switches with interlocking and electromagnetic locking are the XCSLxx range.
XCKJ59xx was available in many variations of solenoid connector and actuator orientation as well as coil voltages and cable gland threads. Not all these combinations are available in XCSLxx switches, but there is usually one close enough for most applications.
There is also a much more up to date range of metal or plastic safety switches with solenoid locking/unlocking, the XCSExx and XCSTExx ranges. However, whilst these perform a similar function the physical design is quite different and may require modification of the machine/mountings to replace XCKJ59xx. Please see the attached document for details.
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Range:
Explore more
Range: