{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number of the fixed Front Connection snap-in nuts for the Compact NS100 to 630 and NSX100 to 630 circuit-breakers?

The part number of a set of 12 fixed front connection snap-in nuts is:

LV429234 for Compact NSX100.
LV430554 for Compact NSX160 and NSX250.

These can fit onto the NS100, NS160 and NS250 MCCBs as well.

These parts are not available for Compact NS400 to 630 and NSX400 to 630 MCCBs.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: