Search FAQs
What are the advantages of the ZBPA, ZBP0 and ZBP0A clear pushbutton covers for the Harmony XB4 and XB5 range pushbutton switches?
Rubber boots provide additional protection against the following:
Here is the list of part numbers for our boot covers:
A cover cannot be used with a legend holder. Clear, round, self-adhesive legends are required (type ZBY1101).
- Dust / dirt / grime build-up
- Some protection against water build-up, which could cause units to freeze in certain environments
Here is the list of part numbers for our boot covers:
- ZBPA: covers for flush pushbuttons with circular head
- ZBP0: covers for projecting pushbuttons with circular head
- ZBP0A: covers for flush or projecting pushbuttons with circular head for food & beverage applications
A cover cannot be used with a legend holder. Clear, round, self-adhesive legends are required (type ZBY1101).
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: