Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How does the "Dead man's switch" or "Dead man's handle" position work on a controller handle?

Please note that we no longer sell joysticks, so this FAQ is for information only. 

Technological description

The handle grip comprises a fixed part (lower section) and a moving part (upper section).
Action on the upper part of the handle grip (pressing down) drives a sliding rod inside the control lever.
This rod actuates a moving retainer which causes a change in electrical state of the contact element on the lower part of the mechanism, regardless of the position of the control lever.
 

Operation

In normal operation, the operator must maintain pressure on the handle grip to operate the machine.
If the operator releases pressure (e.g. feels ill and passes out), even if they are still holding on to it, the electrical contact at the base will change state. 

Dead Man

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more