{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between AC-7a and AC-7b when choosing a iCT contactor?

These utilization catagories determine what load the contactors are switching:
AC-7a are for slightly inductive loads for household appliances for example mixers and blenders
AC-7b are for motor-loads for house hold appliances such as fans and central vacuums

The following is an extract from the IEC EN 61095 detailing the Utilization catogories for Electromechanical contactors for household and similar purposes
EN 61095 Mar2009 Table 1 Utilization Categories

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.