{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why does the PM5110 (METSEPM5110) meter display incorrect power readings or not show any current?

The connections from S1 and S2 on the current transformer to I+, and I- on the back of the meter might be reversed, ensure that the wiring of the meter is correct as per the user manual

Incase of using a stand alone CTs, ensure the P2 is facing the load

Ensure that the meter has been programmed (e.g CT ratio , System Type)

S1 and S2 connections may still have the link in, (Please remove this while power is OFF)

Please note that this relates to all Meters from the Power Logic PM5000 range.

Schneider Electric Ireland

Attachment(s)

PM750 user manual.pdfPM750 user manual.pdf [2.74 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: