{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the largest outgoer for a SEA9BN Distribution board ?

The Maximum out going circuit breaker fitted in to the board under normal conditions is 63amps iC60 circuit breaker.

It may be possible to externally mount a iC120 circuit breaker in a extension box SEA9BNEX034N, and use lug unit SEA9TB1001 ( Max 100A  rated ) ( Qty 3 ) to take current from the board and into a iC120 breaker. But the maximun Amperage will then be 100A.

Maximum cable size from neutral bar is 25mm CSA.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: