{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Logic Instruction Capacity In PICED?

The PICED software is the programming interface for C-Bus embedded devices.
The PICED software is the programming interface for CBUS
The Logic Instruction Capacity In PICED is used to allow more than the recommended instructions in the logic engine.

The maximum amount of instructions can be increased within the Logic engine by going to Tools -> Logic Options -> Errors tab.

This is also generally a sign though that the amount of logic on the unit is reaching its capacity

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: