{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we offer a 400mm extension box for Powerpact 4 boards?
We do not offer a 400mm extension enclosure as a spare. We only offer the MG6CEX which is 200mm height, you will need to use 2 of these to give the 400mm Height, these can be double stacked.  MG6CEX can only be fitted to the MG2C# ,MG6C# and the MG8C# boards. MG6CEX cannot be fitted to the MG25C# and the MG16C14 boards

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.