{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
High harmonic distortion shown on the neutral conductor (PM820)
Possible that the load is causing a disturbance on the current harmonics.

If the load measured by this meter has a high 3rd and 9th harmonics, the "neutral harmonics", they are not cancelled among the phases and just drained to the neutral line. This explains the image where this harmonics represents about 20% to 30% of the fundamental current on the lines, but they are more than double the fundamental on the neutral.

The typical loads that causes this disturbance are switched power supply (computer/servers) connected on Line to Neutral plugs.

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.