{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In the Compact NSX Range, can I use a Basic Frame with Trip Unit removed as a Switch Disconnector?
NO this is not permitted at all -  Switch disconnectors must be ordered as a full unit

The Frame is only one part of a Breaker and it needs a trip unit fitted inside to create a complete device

The Frame cannot function as a switch on its own without a trip unit as their is no continuity across the poles






Schneider Electric Ireland