Search FAQs
What are the Zs values for MGP style breakers
The MGP style breakers are NSX breakers with an atatchment devive for Powerpact 4 boards.
The Zs values for MGP breakers are the same as the equivalent NSX breaker,
Please see the attached files, for the NSX range with the Cmin factor added.
eg - Zs for NSX 160A = 0.15 @ 0.4 s and Zs for MGP160 = 0.15 @ 0.4s ( 0.95 factor not applied).
The Zs values for MGP breakers are the same as the equivalent NSX breaker,
Please see the attached files, for the NSX range with the Cmin factor added.
eg - Zs for NSX 160A = 0.15 @ 0.4 s and Zs for MGP160 = 0.15 @ 0.4s ( 0.95 factor not applied).
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Range:
Explore more
Range: