Search FAQs
Can the trip units be set in-between settings?
The NSX thermal magnetic trips can only be set at the incremental settings provided, they cannot be set mid way between points.
For example, the Im shown below can only be set to 1250, 1500, 1750, 2000, 2250 or 2500 Amps. Therefore, it is not possible to set to 2100A .
![Setting dials on Micrologic Trip unit](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000AVz7aQAD&oid=00DA0000000abSmMAI)
This is true for all the ranges of the Micrologic Trip units
For example, the Im shown below can only be set to 1250, 1500, 1750, 2000, 2250 or 2500 Amps. Therefore, it is not possible to set to 2100A .
This is true for all the ranges of the Micrologic Trip units
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: