{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum cable installed on SEA91253N/SEA91254 125A incomer?

The Maximum cable size for the SEA91253N & SEA91254 is 50mm2 rigid cable or 35mm2 flexible or with ferrule cable.

For installation of a 70mm2 cable you would require a larger incomer such as 160A, 200A or 250A.

Schneider Electric Ireland

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: