Search FAQs
Which combination block is used for circuit-breaker and contactor mounted on the LAD311 mounting plates?
LAD311 is a mounting plate designed to accept the following devices mounted together:
If it is an LC1K range contactor, the combination block to be used between this range of contactors and the above circuit-breakers is GV2AF01. However, GV2ME/GV2P + Tesys K contactors combined cannot be mounted on LAD311 plate.
- GV2ME/GV2P circuit-breakers,
- TeSys D range contactors: LC1D09-LC1D38, The combination block to be used to link the power connectors of the two devices prior to mounting, is part number GV2AF4.
If it is an LC1K range contactor, the combination block to be used between this range of contactors and the above circuit-breakers is GV2AF01. However, GV2ME/GV2P + Tesys K contactors combined cannot be mounted on LAD311 plate.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: