Search FAQs
Is Zelio Soft software compatible with Windows Vista and/or Windows 7, Windows 8 and Windows 10?
Zelio Soft V5.4.2 is compatible with the following:
Since Zelio Soft V4.5, it has been compatible with Vista and Windows 7 (W7). However, most installations of Vista and W7 are 64 bit and ZelioSoft V4.5 did not include a 64 bit cable driver, which had to be installed separately (downloadable free of charge from www.se.com/uk)
Note: V4.5 is not compatible with W8.
Zelio Soft V4.6 was released June 2015 , which is compatible with Vista, W7, W8 and now includes the 64 bit driver.
- Windows 7 32bit
- Windows 7 64bit
- Windows 8.1 32bit
- Windows 8.1 64bit
- Windows 10 32bit
- Windows 10 64bit
Since Zelio Soft V4.5, it has been compatible with Vista and Windows 7 (W7). However, most installations of Vista and W7 are 64 bit and ZelioSoft V4.5 did not include a 64 bit cable driver, which had to be installed separately (downloadable free of charge from www.se.com/uk)
Note: V4.5 is not compatible with W8.
Zelio Soft V4.6 was released June 2015 , which is compatible with Vista, W7, W8 and now includes the 64 bit driver.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: