{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

With the TSXCUSB485 cable, which Unitelway driver should I install for use in Windows Vista Business Edition 32?

The Unitelway V2.0 IE10 driver needed for the various Schneider programs which use the Unitelway protocol (PL7 Micro/Junior/Pro, Unity Pro , Control Expert, Vijeo Designer Lite) is available in the attachments.

It supports the following:
  • TSXCUSB485 USB cable
  • TSXPCX1031 serial cable.

This attachment is an executable file which includes:
  • The Unitelway driver
  • The USB bus Windows driver
  • The virtual serial port Windows driver

Note:
This executable is found in the V2.6 pack driver.

Schneider Electric Ireland

Attachment(s)

SchneiderUnitelwayDriverVista32.zipSchneiderUnitelwayDriverVista32.zip [9.3 MB]