Search FAQs
What is the correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket?
The correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:
![Cable colours for VW3A8306D30 cable Cable colours for VW3A8306D30 cable](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H0000088Z9IQAU&oid=00DA0000000abSm)
Please note that the Modbus serial connection function of each pin is as follows :
Pin number 4 (D1): blue wire
Pin number 5 (D0): white-blue wire
Pin number 8 (0 VL): brown wire
Please note that the Modbus serial connection function of each pin is as follows :
Pin number 4 (D1): blue wire
Pin number 5 (D0): white-blue wire
Pin number 8 (0 VL): brown wire
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: